1/16/2019 5:36 AM | |
Posts: 33 Rating: (0) |
I've tried to see the overview from command prompt and this is what happened. Any help will be appreciated. Thank you. |
1/16/2019 10:13 AM | |
Posts: 33 Rating: (0) |
Hi, I'm not sure if this is Engineering sample or MindConnect IoT. Below is the attachment |
1/16/2019 10:28 AM | |
Joined: 4/28/2015 Last visit: 8/26/2024 Posts: 3345 Rating: (379)
|
Hi, this is a SIMATIC IOT2040 - the correct device. If you have flashed the image (Example_Image_V2.2.0 downloaded from here) correctly according to the setting up and your LAN settings are correct, I can't imagine that.. Please check if the µSD card is plugged in correctly like this: Have you already tried to flash the image again or to use another µSD card? Which tool are you using to flash the Example Image to the µSD card? Best regards! |
Last edited by: bergmanu at: 1/16/2019 10:29:29 AMtypo Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on