1/25/2023 7:35 PM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33954 Rating: (4221)
|
Have you allowed the Modbus access in the file properties? |
1/26/2023 5:58 AM | |
Joined: 3/30/2020 Last visit: 10/14/2024 Posts: 4867 Rating: (995) |
That is what the photo says. And you may be right. The LOGO! should 'process' or 'display' the values from the "Smart Logger". My standpoint is that the LOGO! is providing the inputs/outputs for the logging action provided by his device. But that says he does not want to use the functionality the LOGO! gives to log data. Also I have no clue what this "Smart Logger" is. So my side of the guessing opinion also could fail. Perhaps now the topic starter understands there is help available on our forum but he needs to give us the "eyes" to see. Good day to you. Add |
Last edited by: qwazee at: 01/26/2023 06:02:02Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
4/18/2023 11:01 AM | |
Joined: 4/18/2023 Last visit: 4/18/2023 Posts: 1 Rating: (0) |
Open TCP connection at inverter Huawei |
Follow us on