7/6/2007 3:20 PM | |
Posts: 25 Rating:
|
Dear experts I have a PC with two Normal ethernet cards. AttachmentMAC Bridge.zip (693 Downloads) |
7/7/2007 10:09 PM | |
Joined: 1/7/2006 Last visit: 12/23/2024 Posts: 2705 Rating:
|
Hi, Have you read the S7-APRED documentation... AttachmentAPRED S7.pdf (665 Downloads) |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
7/11/2007 2:00 PM | |
Posts: 25 Rating:
|
Dear experts, Thankyou very much for your valuable suggestions. In case if i have only one Ethernet card in the PC(No bridging concept) and two CP 443-1 in the 412 CPU rack, ie Ethernet card is connected to Switch and the CP443-1 are also connected through the same switches, whether i will be able toremain online if one of the CP 443-1 fails?? AttachmentNo mac bridge,only 2 CP443-1in CPU rack.zip (672 Downloads) |
Follow us on