1/31/2017 9:22 AM | |
Joined: 12/18/2014 Last visit: 10/8/2024 Posts: 33906 Rating: (4216)
|
In the attachment is a video showing how to connect 2 LOGO!s 0BA8. The complete video is now in my post further down,from 10/12/2018 9:42 AM. |
Last edited by: ixo65 at: 10/12/2018 11:01:22 AM |
|
This contribution was helpful to1 thankful Users |
1/31/2017 9:28 AM | |
Joined: 12/18/2014 Last visit: 10/8/2024 Posts: 33906 Rating: (4216)
|
And here the second file of the ZIP Archive. For the second archive to be uploaded, I had to rename it. After downloading this file "2 Logo 0BA8 connected.z01.zip" you have to rename it into "2 Logo 0BA8 connected.z01". The complete video is now in my post further down,from10/12/2018 9:42 AM. |
Last edited by: ixo65 at: 10/12/2018 11:02:00 AM |
|
This contribution was helpful to1 thankful Users |
10/12/2018 9:25 AM | |
Posts: 6 Rating: (0) |
Hi, I have problem to extracts files. Not find the file 2 Logo 0BA8 connected.z01 and if I change the name this file remain .zip |
10/12/2018 9:42 AM | |
Joined: 12/18/2014 Last visit: 10/8/2024 Posts: 33906 Rating: (4216)
|
Everything is alright with the ZIP files, I just tested. Attachment2 Logo 0BA8 connected.wmv (1703 Downloads) |
Last edited by: The Helping Hand at: 10/12/2018 10:00:07 AMAdded video |
|
This contribution was helpful to2 thankful Users |
Follow us on