3/10/2020 2:53 PM | |
Posts: 9 Rating: (0) |
I would like my RTU to be able to read the value of the LOGO! network output function block which i have set to VB:1, bit: 1 |
3/10/2020 3:03 PM | |
Joined: 12/18/2014 Last visit: 5/12/2024 Posts: 33019 Rating: (4079)
|
Who ist the server, who is the client? |
3/10/2020 3:09 PM | |
Posts: 9 Rating: (0) |
i am communicating Modbus/TCP to a remote device which is an RTU (data concentrator) |
3/10/2020 3:22 PM | |
Posts: 9 Rating: (0) |
I came across this in another post. i will try this addressing schedule; see attached pdf which i believe implies V1.1 will be at coil 10: AttachmentModbus Table.pdf (375 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on