6/26/2009 3:21 PM | |
Joined: 7/2/2008 Last visit: 9/30/2024 Posts: 928 Rating: (309) |
Hello Thinker, For latest frimware updates, check this link. Firmware update doesn't increase work memory of CPU and if you have problems with 256KB, I'm afraid that you might need to go for bigger CPUs. However,I think 256KB is quite enough for such CPU. Why do you think you may need more capacity? Best regards. H-H |
7/3/2009 9:35 AM | |
Joined: 3/21/2006 Last visit: 1/14/2025 Posts: 10239 Rating: (1182) |
Hello Olof, MLFB is order number of SIMATIC S7/S5 products. Each product has own MLFB number like 6ES7331-1KF01-0AB1. Each letter in this number has own meaning. Here we already discussed this meaning and end result came from Pegaia. He wrote:
Regards Hristo Mihalev |
7/3/2009 9:48 AM | |
Posts: 8946 Rating: (999) |
Maschinen Lesbare Fertigung Bezeichnung. |
7/4/2009 9:25 AM | |
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating: (237) |
Thanks Hristo for this information. |
7/4/2009 9:53 AM | |
Posts: 8946 Rating: (999) |
Hi Lalit, there is also a "Thank" Button in the upper right corner of any post - box. It is easy to use, just try it! |
This contribution was helpful to1 thankful Users |
Follow us on