4/23/2021 6:13 AM | |
Joined: 8/25/2006 Last visit: 4/27/2024 Posts: 2203 Rating: (277)
|
Hello. Add new IM to Profibus in HWConfig, add required modules to the IM. Configure CRV/CTV for this IM in CFC and virtual connections as discussed earlier. Instead virtual connections you can use pointer-based communication (CRV_P/CTV_P), look at sample project in Simatic Manager 'D7-TDCbasic', D01P01, Chart 'Com_Profibus'. |
This contribution was helpful to1 thankful Users |
4/23/2021 8:34 AM | |
Joined: 6/19/2017 Last visit: 4/26/2024 Posts: 7957 Rating: (162) |
Closed cause question posted twice. The second thread with the subject How to install new AI card in IM153 and its configuration in TDC side? is published within the conference SIMATIC TDC, FM458, T400. Jen_Moderator |
My Forum is the place to personalize your profile, |
|