Industry Online Support
Technical Forum
3/8/2012 3:41 PM | |
Posts: 3037 Rating: (192)
|
Hello, The benefit of the RDB log is this log is faster as CSV log or TXT log. See the chapter 3 in the following link. How are tags and alarms logged in WinCC flexible? You have still anotherbenefit at the new Comfort Panel with RDB logs. See the following link. What are the functional differences between the different log storage locations in the SIMATIC Comfort Panels and Runtime Advanced? Tweety |
This contribution was helpful to1 thankful Users |
3/9/2012 7:51 AM | |
Posts: 327 Rating: (28) |
Greetings RDB format is actuallySQLitedatabase. To an end user, there is no much difference. But if you want to analyze it or something externaly, you can use SQL queries on it. Best regards
|
This contribution was helpful to1 thankful Users |