3/14/2010 12:58 PM | |
Joined: 3/14/2010 Last visit: 11/28/2023 Posts: 4 Rating: (0) |
Hello all download link www.slsgroup.ru/s7200sim/s7200sim/Download/tabid/79/language/en-US/Default.aspx Simulator work together with STEP7 MicroWIN. It is possible to download, upload, debug (program & status chart) directly from MicroWIN. |
This contribution was helpful to4 thankful Users |
10/19/2014 6:16 PM | |
Posts: 2 Rating: (0) |
Dear sir, can you send me english version site to download s7 200 plc simulator this is because i am unable to read above language
|
10/20/2014 12:14 PM | |
Joined: 3/14/2010 Last visit: 11/28/2023 Posts: 4 Rating: (0) |
Good day. Setup in the attachment.
AttachmentSetupEng.zip (4072 Downloads) |
10/25/2014 2:38 PM | |
Joined: 3/14/2010 Last visit: 11/28/2023 Posts: 4 Rating: (0) |
The problem is Windows CodePage 1252. Try new help. Briefly: you have to set-up link between S700SIM and MicroWIN by the virual COM port pair. Then you will work with simulator like with real CPU (download program, send RUN,STOP commands, use watch tables, e.t.c.
AttachmentHELP2014.zip (1185 Downloads) |
This contribution was helpful to1 thankful Users |
4/14/2015 6:49 PM | |
Posts: 2 Rating: (0) |
I use google translate for the page http://www.slsgroup.ru/s7200sim/s7200sim/Download/tabid/79/language/en-US/Default.aspx nbut I got an error Page not found |
Follow us on