5/29/2012 3:49 PM | |
Joined: 8/31/2010 Last visit: 3/16/2023 Posts: 1498 Rating:
|
Hello TIM77, I have mistaken valve as value. Let's leave that apart, ignore my prev post. Hope you have two images configured under a Graphics List and you are displaying it using a Graphics IO Field (Output mode). Is this right? In this case create a new button and choose the option Invisible mode in the button. Then size the button with same dimensions of the Graphics IO field and place the button exactly above it. Now you can configure events for this invisible button and assign any event as you wish. It will look like a Graphic in the Runtime, but still you can touch it to do the ON / OFF functionality. Hope this helps. Many more possibilities can be found at - Demo Project for Comfort Panels |
Like it? Rate it! |
|
This contribution was helpful to
1 thankful Users |
5/29/2012 4:01 PM | |
Joined: 5/7/2012 Last visit: 3/23/2023 Posts: 35 Rating:
|
Thanks Ganse10. I think this solves my problem |
Follow us on