10/24/2019 9:08 AM | |
Joined: 12/18/2014 Last visit: 5/8/2024 Posts: 32991 Rating: (4076)
|
I did tests. From this it can be seen that the data log is also written if the buffer is not yet filled with 512 bytes. Data Logs are attached. AttachmentData Logs.zip (255 Downloads) |
10/24/2019 10:26 AM | |
Joined: 12/18/2014 Last visit: 5/8/2024 Posts: 32991 Rating: (4076)
|
Here have news. AttachmentData Logs.zip (183 Downloads) |
10/24/2019 2:57 PM | |
Posts: 7 Rating: (0) |
Thanka all for replyes. 1. When I trying get DataLog via LSC I receive massage "No datalog found". 2. If I stop Logo and remove SD Card and read them in PC then I found zero length csv file (Program worked 1 week before read SD card) 3. Programm and screenshot of DataLog block properties is attached. AttachmentData Logs.zip (182 Downloads) |
10/24/2019 3:30 PM | |
Joined: 12/18/2014 Last visit: 5/8/2024 Posts: 32991 Rating: (4076)
|
Hello Nopolis, please be so Kind and upload you program as a ZIP file. Thanks. |
10/24/2019 6:25 PM | |
Posts: 7 Rating: (0) |
Program in attached zip file
AttachmentVer 9.zip (189 Downloads) |
This contribution was helpful to1 thankful Users |
10/24/2019 7:19 PM | |
Joined: 12/18/2014 Last visit: 5/8/2024 Posts: 32991 Rating: (4076)
|
First transferred your uploaded program to my LOGO! 8.FS4. In attachement: AttachmentData Logs.zip (184 Downloads) |
10/24/2019 8:13 PM | |
Joined: 2/22/2008 Last visit: 5/8/2024 Posts: 2698 Rating: (206) |
Once again a destroyed program, which can be uploaded to the Logo and don't have all functions. |
10/24/2019 8:23 PM | |
Joined: 12/18/2014 Last visit: 5/8/2024 Posts: 32991 Rating: (4076)
|
I suggest the User Nopolis to start a Support Request so that Siemens will examined his source program. |
This contribution was helpful to1 thankful Users |
Follow us on