9/5/2024 10:05 AM | |
Joined: 2/17/2020 Last visit: 9/6/2024 Posts: 1047 Rating: (190) |
Hi, yes, there is no longer an MPI interface for the S7-1500 and S7-1200. Please see: Migration Guide: SIMATIC S7-300/400 to SIMATIC S7-1500 There are a few gateways, but it is not a Siemens solution. I believe that a Profibus CP or CM can also be used. It should be noted that the connected Profibus network is "set" to MPI. However, this must be done by hand. |
A rating will be well appreciated. |
|
This contribution was helpful to1 thankful Users |
9/5/2024 3:13 PM | |
Joined: 1/25/2023 Last visit: 9/5/2024 Posts: 6 Rating: (0) |
thank you |
Follow us on