4/5/2017 4:26 PM | |
Joined: 2/6/2015 Last visit: 9/26/2024 Posts: 3 Rating: (0) |
Hi, After installation of TIA V13 + SP2 there are no interfaces available in control panel 'Set PG/PC Interface' OS is Windows 10 Pro x64 From viewing other threads here I've tried the following:- Reinstall TIA V13 SP2. Delete the C:\ProgramData\Siemens\Automation\Simatic OAM\data directory, open cmd (admin) window and run s7epaIMP64x.exe from that prompt (log attached) But still no joy. Any help would be appreciated, cheers J Attachments7epaImp64x_2017-04-05.11.49.45 .txt (494 Downloads) |
Last edited by: jm_atlast at: 4/5/2017 4:27:42 PM |
|
Follow us on