2/5/2019 1:01 PM | |
Joined: 4/28/2015 Last visit: 10/9/2023 Posts: 394 Rating:
|
Hello, did you try to use function block "CTRL_HSC_EXT" with HSC structure: -> NewStartValue (IN - Dint) StartValue = Initial value of the HSC For more information, have a look into System manual V4.2.3 (08/2018) at chapter 10.1.1.3 and following... |
2/5/2019 6:41 PM | |
Posts: 2826 Rating:
|
Hello.
There has been changes since 2016 in the HSC functionalities. The hardware configuration for firmware now is different than earlier versions. The changes are for the better. Attachmentinitial-and-sync-input.pdf (305 Downloads) |
Follow us on