8/10/2011 1:37 PM | |
Joined: 8/10/2011 Last visit: 6/5/2024 Posts: 26 Rating: (0) |
Any solution? |
8/10/2011 4:00 PM | |
Joined: 8/10/2011 Last visit: 6/5/2024 Posts: 26 Rating: (0) |
Hi First of all, thank you very much for your fast reply. I've tried cutting and it works. But it should work copying the charts because the CFC help points in this way (I attach the )and because I (and other colleagues)did itwith PCS7 V7.0 in the past. It's very useful for replicating functional units of the installation, because I canmodifythe textual interconnection in the destination project with the equipment tags of the new unit I want to create, and then copy back to the source project and close them. It's very strange because it's a very powerfultool. Best regards AttachmentCopy-move charts.pdf (126 Downloads) |
8/12/2011 4:19 PM | |
Joined: 5/18/2006 Last visit: 10/21/2020 Posts: 170 Rating: (63) |
This issue is corrected with the CFC V7.1 SP2 Update 1 (http://support.automation.siemens.com/US/view/en/45947417). cabreytj |
8/16/2011 9:32 AM | |
Joined: 8/10/2011 Last visit: 6/5/2024 Posts: 26 Rating: (0) |
Hi It works. Thank you very much. |
Follow us on