3/28/2023 10:41 AM | |
Joined: 10/22/2020 Last visit: 7/11/2024 Posts: 169 Rating:
|
Hey, as you mentioned in the first post, your updated blocks require a node version > 15. I assume that you currently have these blocks active in one of your flows and that this is causing NodeRED to fail on startup. So please try to start Node-RED without starting the flows. This allows you to open the faulty flow in the editor and make changes without running anything. When you deploy your changes, the flows are then started:
Following these instructions, it is possible to update Node and NodeRED. Please note that newer versions of Node and NodeRED can have a significant impact on all packages you have installed so far, and you may encounter difficulties elsewhere in favour of the more recent OCPUA modules. BR |
Follow us on