12/16/2016 4:54 AM | |
Posts: 6 Rating: (0) |
meta-iot2000/meta-iot2000-example/recipes-node/node-red/node-red_0.14.6.bb maybe this file not call npm-shrinkwrap.json then , iot2000-example-image dont work node-RED |
12/16/2016 10:50 AM | |
Posts: 6 Rating: (0) |
Thank you for reply. After tomorrow, download and build. |
12/16/2016 2:18 PM | |
Posts: 40 Rating: (2) |
Hi Yoshidaw, seems like you are building the image on yourself. Did you try to include the node-red recipe to the image? Take at look at this file in the staging branch: meta-iot2000/meta-iot2000-example/recipes-core/images/iot2000-example-image.inc IMAGE_INSTALL_append = " node-red node-red-dashboard node-mraa node-red-node-intel-gpio" Then you can build your image with node red even today ;) |
12/17/2016 1:53 PM | |
Posts: 6 Rating: (0) |
Thank you for helpful information. In addition to node - RED, if the file may be updated, wait for Taxflor 's file update.
|
12/19/2016 9:32 AM | |
Joined: 1/26/2011 Last visit: 8/11/2022 Posts: 243 Rating: (67)
|
Hello together, You can find the latest features in the following post: The most important feature for this forum thread is, that node-red is preinstalled now in the version 2.1.2 of the example image.
|
Follow us on