4/4/2022 10:05 AM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hi, chapter 3.4 describes the update of the firmware. The firmware V1.2.1 is a pre-condition for using the Example Image V1.2.1/V1.2.2, which has NodeJS 12. Firmware and Example Image are two different things.
I am always using SD card. You need an SD card to change the content of the eMMc, because you cannot change the image on the eMMc while running the image from eMMc.
Chapter 3.2 describes clearing the eMMc in case Example Image V1.0.2 or Industrial OS is running on the eMMc. The reason is that those images are not running with the firmware V1.2.1. Clearing the eMMc can only be done while running an OS from SD card. After this you need to write an Example Image to the eMMc again (see here) Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
4/4/2022 10:44 AM | |
Joined: 3/18/2021 Last visit: 1/24/2024 Posts: 31 Rating: (1) |
Ah ok, thank you very much for the explanation.
Is it possible to check, if V1.0.2 is running on my eMMc, so I can skip that part if it is not? Is there a guide on how to change the Example Image after updating the firmware? |
4/4/2022 2:25 PM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hi, the usual way is to check it via cat /etc/os-release, which is not possible anymore in your case. The way to boot from an SD card and change firmware: - Run your current image from eMMc
- Write Example Image to an SD card (described here)
- Follow this guide to write Example Image to eMMc again Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
4/5/2022 9:56 AM | |
Joined: 3/18/2021 Last visit: 1/24/2024 Posts: 31 Rating: (1) |
Ok, so let me sum up, what I have to do to have the Example Image V1.2.1: At first I clear the eMMc. For that I change the boot order. My boot order looks like this now:
I have the Example Image on a USB Stick so I would use USB instead of an SD card. Then I follow this steps: I clear the eMMc and write it again with the Example Image V1.1.1 right? Instead of an second USB stick can I use WinSCP to transfer the Example Image file to the IOT2050?
After that I have to update the firmware on the eMMc. For that I plug out the USB Stick and boot from the eMMc. I use this manual to do that. I can skip chapter 3.2 (Clear eMMc) because I already did that. After successfully updating the firmware I have to write the new Example Image (V1.2.1). I would like to use V1.2.1 instead of V1.2.2 because I know that Node-RED will work there. Where can I find Example Image V1.2.1? I only found V1.2.2 in the download section. And how do I overwrite the new Example Image to existing one?
After that I just have to remove the USB Stick and boot from the eMMc and can use V1.2.1 correct? Is this method correct or did I forget something or did it wrong? Thank you very much in advance! Best regards |
Follow us on