11/25/2017 3:20 PM | |
Joined: 9/27/2006 Last visit: 10/2/2024 Posts: 12283 Rating: (2685) |
Hello Mohsenm; To set things up properly, I have to say I am not an expert on Logo! So first, here is a discussion on the forum considering ways to handle non-linear sensors of S7 CPUs; please take the time to look at proposed solutions: Of course the mentioned CPUs of the S7 family have more available memory and a larger instruction set than the Logo!. The only alternative I have found in Logo! is the look-up table technique, and here is a thread discussing the issue: https://support.industry.siemens.com/tf/fr/en/posts/lookup-table-in-fbd/164869/?page=0&pageSize=10 Hope this helps, |
This contribution was helpful to1 thankful Users |
Follow us on