Industry Online Support
Technical Forum
5/9/2011 5:05 PM | |
Joined: 9/23/2005 Last visit: 3/24/2023 Posts: 4180 Rating:
|
Hi, The installation of STEP 7 V11 is relatively simple. Here there is the sequence of a normal installation. It could be used as compare base, if some problem occurs. Attached there is the print screens of the installation pictures 0 - Insert the DVD on the PC. If it doesn’t start automatically, click on start.exe 1 - If you don’t have .NET installed, it will ask you to do it. 2 – After the installation of .NET, it will ask to restart the Windows 3 – It asks to set the installation language (not the SW language). 4 – It asks to set the SW languages (not the installation language). 5 - It asks about the additional components (normally the typical configuration – default – is enough). 6 – It asks to accept the license terms 7 – It asks to accept the changes that it will perform (for example user rights, regedit settings) 8 – It asks to confirm the installation 9 – It asks if you would like to transfer the license now (if you want, it is possible to transfer the license after the installation). 10 – It asks to restart the Windows. Attachmentpictures.zip (318 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
3 thankful Users |
Follow us on