10/7/2020 1:20 AM | |
Joined: 3/12/2019 Last visit: 11/22/2022 Posts: 1 Rating: (0) |
Hi, im having kind of the same problem, i was hoping you could help me. I´m also running WinCC Pro, I did testing on a Windows 10 PC with WinCC RT and the communication worked great, nevertheless I migrated the project to a Windows 10 Server, and I'm no longer able to see any of the PLC Values. I read about the SIMATIC NET PC Software and that I might be missing that installation but its curious since I never installed this software on the other PC (which is also different as the engineering one). Also another change was that I used different networks but both, Server and PLC are visible between them i have tested this by doing PING via terminal The Communication setting on the Tia Portal is the following: RT PC IP ADDRESS: 10.5.129.104/24 Router: 10.5.129.1 PLC: IP ADDRESS: 10.5.144.52/24 Router: 10.5.144.1 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/07/2020 10:32:08New subject after splitting |
|
Follow us on