Industry Online Support
Technical Forum
10/1/2021 12:06 PM | |
Joined: 4/23/2020 Last visit: 7/23/2024 Posts: 5 Rating:
|
Hi i was using PCS7 v9.0 and wincc 7.4 in this wincc runtime screen footer simatic batch icon was there, if i click means simatic batch will open, so now wincc scada runtime and batch screen was opened in single screen but i cant able to switch to second monitor, if i open the simatic batch from control center means i can able to switch to second screen, is there any setting i need to do for the same in winncc. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/01/2021 13:14:45New subject after splitting |
|
Follow us on