8/22/2022 11:56 PM | |
Joined: 9/27/2006 Last visit: 5/25/2024 Posts: 12257 Rating: (2668) |
Hello mattar; Have a look at this information: https://support.industry.siemens.com/cs/ca/en/view/90156662 "You cannot do a complete upload of the Technology because the system variables, unlike configuration data, cannot be transferred from the Technology back into the PG/PC". Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
8/23/2022 11:41 AM | |
Joined: 10/4/2017 Last visit: 4/21/2024 Posts: 40 Rating: (3) |
Thank you for your contribution. Do I have to uninstall starter and install S7-technology to upload the blocks?
|
8/23/2022 11:54 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985) |
is the PLC dispalyed in the HWCatalog of your installation? |
8/23/2022 12:24 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985) |
yes uninstall starter and install s7-technology |
Follow us on