2/9/2017 2:27 PM | |
Posts: 4 Rating: (1) |
Hi everyone, What is the maximum number of devices I can connect to an 1515-2PN CPU through Modbus TCP/IP? Where can I find this information? Thanks in advance! |
2/23/2017 3:47 PM | |
Posts: 3093 Rating: (323) |
Hello, You did not tell us a main thing: does the S7 act as client or server? Regards, |
2/23/2017 4:07 PM | |
Posts: 41 Rating: (3) |
It does both, i have somefing like 10 big tree of cpu. and some stations communicates with this 10 cpu in the same time. (I use ModBus for the opening protocol) This FAQ just say we can't have 10x MB_SERV on S7-1x00 in the same port. i have no issues at the moment, i use multi-port. But Is just to see if someone doing a better management/code |
Last edited by: ASI_ab at: 2/23/2017 4:13:56 PM |
|
5/4/2021 9:04 AM | |
Joined: 11/8/2017 Last visit: 1/17/2024 Posts: 22 Rating: (0) |
Hello, nothing is said in the manual or catalog. But in the TCP/iP network, there are no restrictions on the model s7-1500 Read the manual. https://support.industry.siemens.com/cs/attachments/109763260/s71500_s71500f_et200mp_product_information_en-US.pdf?download=true |
Last edited by: Jen_Moderator at: 05/04/2021 10:34:30Removed links, because it's an advertisement. |
|
Follow us on