Industry Online Support
Technical Forum
6/30/2013 4:57 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating:
|
Hi, yes that is a problem of the LAn-connection in the Master-slave mode. Short input pulses can be lost or you must input longer pulses until the master get a new aktual information of the input states of the slave. To solve this use a master-master modus. Then can you analyze the inputs with a smal program. If you do this the input pulses can be short and would be "memoried" a little time or you use a digital merker or an unused output to send a signal to the other master (befor this was the slave) to clear all memoried inputs... Best regards Betel |
==> Meine TAG-Listen: "deut." |
|
Follow us on