Industry Online Support
Technical Forum
12/14/2009 12:49 PM | |
Joined: 9/27/2006 Last visit: 5/21/2024 Posts: 12257 Rating: (2668) |
Hello nevertheland; In the technical specifications of the OLM-4 manual, it is mentionned that the OLMs are of protection class IP 40: http://support.automation.siemens.com/WW/view/en/24164176 So you have no protection against dusty environments or water. It looks like your plan to place them in an IP 65 enclosure would be advisable if your workplace is dusty. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
12/15/2009 9:23 AM | |
Joined: 12/9/2009 Last visit: 4/18/2024 Posts: 156 Rating: (11) |
Hello, there are the SIPLUS OLM V4. Lock at the release of delivery where you can find more information and contact person for SIPLUS: http://support.automation.siemens.com/WW/view/en/29677409 Maybe it helps you. |
Follow us on