Industry Online Support
Technical Forum
1/2/2009 12:00 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Hi, To your questions the answers: 1. Yes that is possible, a point-to-point connection with two OLM P11; 2. See the handbook of the OLMs: SIMATIC NET PROFIBUS Optical Link Module OLM / P11 V4.0 OLM / P12 V4.0 OLM / G11 V4.0 OLM / G12 V4.0 OLM / G12-EEC V4.0 OLM / G11-1300 V4.0 OLM / G12-1300 V4.0 Operation manual 3. Yes even for 12 MBit/s is that possible; |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on