8/14/2014 12:31 PM | |
Posts: 27 Rating: (0) |
Hello everyone, IPC 477D, there are multiple keyboards running together when in runtime, the windows 7 touch keyboard, the simatic on screen keyboard, and there is that little num pad looking keyboard (usually pops when you are inputting numbers).. some pictures attached . Is there a way to completely disable the simatic keyboards (touch input panel) and only leave the windows 7 one ? there are no settings buttons on those 2 keyboards and the rruntime settings is not helping either. Thank you AttachmentScreen Keyboards.zip (630 Downloads) |
8/20/2014 9:19 AM | |
Posts: 1299 Rating: (136) |
Hello, why do you want to deactivate it? Do they appear simultaneously if you click on an input field? K!ke |
8/28/2014 11:42 AM | |
Posts: 1299 Rating: (136) |
Hello, do you usethe runtime advanced on the ipc? if yes you can use the system function "SetScreenKeyboardMode". K!ke |
8/28/2014 12:21 PM | |
Posts: 27 Rating: (0) |
Hello Kike, Yes, I am using runtime advanced, where is this system function?
|
8/28/2014 12:39 PM | |
Posts: 27 Rating: (0) |
Okay, I will try to do that now. Thank you Kike!
|
4/20/2020 11:01 PM | |
Joined: 7/25/2017 Last visit: 8/8/2024 Posts: 316 Rating: (47) |
I have also encountered lag with keyboard input (although not multiple keyboards popping up). For those encountering such issues in the future, please see the following links; they may be helpful: https://support.industry.siemens.com/cs/fr/en/view/62612047 See heading "Slow response from the screen keyboard and SmartServer": https://support.industry.siemens.com/cs/mdm/92323076?c=62668625419&lc=en-WW |
Last edited by: Jen_Moderator at: 04/21/2020 10:31:42Optimized link. |
|
Follow us on