5/20/2016 12:43 PM | |
Posts: 200 Rating: (6) |
thanks for the reply for some reason i don't get a text field option just root screen |
5/20/2016 12:45 PM | |
Posts: 200 Rating: (6) |
AttachmentDoc1.pdf (183 Downloads) |
Last edited by: Min_Moderator at: 5/20/2016 1:47:15 PMConvert attachment |
|
5/20/2016 1:02 PM | |
Joined: 1/30/2006 Last visit: 4/2/2024 Posts: 310 Rating: (57) |
You have to insert a textbox from your Toolbox, Basic Object. Mark it and se the properties for that object |
BR. Sven |
|
5/20/2016 1:31 PM | |
Posts: 200 Rating: (6) |
how do you create the dummy project as i have tried this but cant see where things are done |
5/20/2016 10:17 PM | |
Posts: 5225 Rating: (1185) |
Hi. For the moment I have no way of knowing what you want to do. If you can ZIP your HMI project and add it here, it might help. It may also help you to look at the project example: Focus on the HMI part of the example. It is not the same device, but much of the workings are the same. Where they use touch buttons, you will use hardware buttons only. Look through the document and work through all the properties of all the elements. It is a bit difficult to explain the fundamentals in text. See if you cannot convince someone closer to you to give you the 30minute kick-start tour. Good luck. |
Follow us on