4/22/2018 9:26 AM | |
Posts: 2 Rating: (0) |
Hi Need help on the 30kW V20 vfd. On start up the drives gives me a A501 fault. parameter r206 reads 22kW and parameter P307 is 30kW and motor driven is a 30kW. The drive specs is 30kW. Could the mismatch between r206 and P307 be the cause of the fault. If yes how can I possibly up r206. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/23/2018 8:09:49 AMNew subject after splitting |
|
Follow us on