12/23/2015 8:04 AM | |
Joined: 10/11/2006 Last visit: 9/9/2024 Posts: 5902 Rating: (803)
|
Hello, depending on the stiff mechanical coupling "two servo motor both with a pinion gear drive the same big spur gear" I would recommend Master "Positioncontolled" , Slave "Torquecontrolled".
Then you don't have the problem with one encoder for 2 TO's.
One possibility is: https://support.industry.siemens.com/cs/ww/en/view/103603156
To twist Master and Slave at standstill, you can give an additional torquesetpoint permanent for the slave (e.g 5% from rated torque; exact value depends on your application)
|
With best regards, |
|
This contribution was helpful to2 thankful Users |
Follow us on