8/14/2024 8:29 AM | |
Joined: 4/28/2015 Last visit: 8/14/2024 Posts: 104 Rating: (22) |
I see what you mean - I have just tried it, and the library UP258 does not allow single-button dimming even though the UP258 datasheet says it does. Do you have to use the UP258? Can you use a standard volt free contact pushbutton instead and combine it with a UP220? Maybe something like the 5TD211? Catalog ET D1 2011 (rs-online.com) |
Follow us on