Industry Online Support
Technical Forum
6/7/2010 9:26 AM | |
Posts: 134 Rating:
|
Hi.. I have one problem with S5 115u cpu 942B. In that cpu, EPROM module of 32kb is installed. Now,i changed onesegment in the program of that cpu. Then one dialogue opens with text " program in eprom , continue? ". I pressed " yes ". Now, when i checked program again that segment is not modified. So, i want to know why it happened. Also, i try by changing program offline and then downloading it in cpu but when i try to transfer same message appears and when i press " yes " , it shows " 0 block tranferred ".That means my modified block doesnt transferred to cpu. So, i want to know that why i couldnt change anything in program of cpu.it doesnt work online or offline. Also if editing is not possible with this cpu, what changes i can do in system to make editing possible?can i use RAM or CPU 943/944. Also, i attached pics of errors for reference. Attachmenterrorrs.zip (56 Downloads) |
6/7/2010 1:09 PM | |
Posts: 24 Rating:
|
I believe that you will have to reburn your EPROM to make the program change. I hope this helps. |
Follow us on