4/23/2018 2:44 PM | |
Posts: 5 Rating: (0) |
I have a couple questions, 1.) When displaying a string value from controllogix on a TP1200 Comfort HMI, I seem to only be able to display a 82 character string. No more, and no less. For instance, if I create a new string in controllogix as String(120) or String(12) (120 characters or 12 character), I get a PLC tag error on the HMI. The string only works when it is a standard 82 character string. Also, it will also not allow me to pick a starting point to begin a string. An example would be if i wanted to start reading the sting at Test.Data(15). When i make this change in the HMI Tag list and download i get the PLC address error. This even happens when the tag i am referencing is the standard 82 character string. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/24/2018 6:51:08 AMNew subject after splitting. Division of questions into separate topics. |
|
4/24/2018 6:53 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating: (169) |
New question published by ChrisWilk is split to a separate thread with the subject How much of a history can display on the trend?. Best regards |
My Forum is the place to personalize your profile, |
|
4/30/2018 8:11 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hey Chris, WinCC Comfort / Advanced doesn't support a communication with Rockwell PLCs. But there exists a FAQ for the communication with a MicroLogix. https://support.industry.siemens.com/cs/ww/en/view/109475773 It could be helpful. With best regards |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
Follow us on