6/21/2016 6:25 AM | |
Joined: 10/12/2013 Last visit: 1/8/2022 Posts: 33 Rating:
|
Dear Davinator, I also facing the problem with OP177B DP mono and couldn't migrate from WinCCFlexible 2008 SP3 UP7 to TIA V11 SP2.Do you have any idea how? Please kindly advise. Thanks, ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/21/2016 9:12:51 AMNew subject after splitting |
|
6/21/2016 10:00 AM | |
Joined: 10/12/2013 Last visit: 1/8/2022 Posts: 33 Rating:
|
Dear, I’m facing a problem with“6AV6642-0DC01-1AX0”OP177B DP MONO HMI project which was created with WinnCCflexible2008 SP3.I did save as WinCCflexible 2008 SP1,SP2,SP3 and tried as well.I had tried to migrate with TIA V10.5 SP2,TIA V11 SP2 and still not successful with getting errors. So far I notice is OP177B not supported in TIA and Please kindly advice for required steps, such as which Simatic HMI is suitable with “OP177B DP mono” matching with existing HMI project? Please see the attached. Your kind help is highly appreciated, Thanks, Min AttachmentMigration_Errors.docx (108 Downloads) |
Last edited by: Dany Min at: 6/21/2016 11:16:35 AM |
|
6/21/2016 12:48 PM | |
Joined: 10/12/2013 Last visit: 1/8/2022 Posts: 33 Rating:
|
Dear Murof, Thanks a lot for your advice. Let me try with WinCC Professional and will update the status. Best Regards, Min |
3/8/2017 11:51 AM | |
Joined: 6/28/2011 Last visit: 2/10/2024 Posts: 111 Rating:
|
Dear Mr. Dany, you converted the HMI from OP177B to which one? |
Follow us on