Industry Online Support
Technical Forum
6/9/2006 2:34 PM | |
Posts: 17 Rating:
|
sirs how do i 'install' an op25 into my s7 project i can't seem to get it to connect to my profibus network |
6/9/2006 4:24 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hello, I suppose you use Protool to programm the panel OP25. There you choose a controller, select the right protocol (profibus) and the right parameters. Then you don't have to implement the panel in the hardware configuration of the S7-CPU. If you use the right profibus parameters on both sides, it will work. But if you want to use DP-Key's, you can download a GSD file. http://support.automation.siemens.com/WW/view/en/113264 Best regards, Wizard |
Follow us on