Industry Online Support
Technical Forum
7/7/2013 12:52 PM | |
Posts: 7 Rating: (0) |
Hi how can I get backup from OP30A 6AV3530-1RR01 ?which software is needed?which cables,ports? regards |
7/7/2013 1:41 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
To whom it is connected? Please find attached sheet, hope it may help you.
AttachmentOP 30 communication cable.pdf (101 Downloads) |
7/7/2013 4:55 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
As it was discassed here -How I can UPloud program from EPROM(OP30B)? |
This contribution was helpful to1 thankful Users |
7/8/2013 9:05 AM | |
Posts: 7 Rating: (0) |
Hi I have connected the op to s5? does the op have internal memory?Or all data is on the EProm? if all data is on EProm,how can I get backup from that? best regards |
7/8/2013 9:34 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, Please follow this link, may be useful to you. |
Follow us on