2/12/2010 5:43 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello esem2704, Unfortunately you can't upload complete project from OP77A using WinCC Flex. software. Reason for that is this type of panel doesn't support retransfer of configuration. The only possible way is to make upload of project (only backup, not editable, restore on the same type of panel) is using Prosave ( Backup/Restore with ProSave). Hope this will helps. Best regards, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
2/13/2010 1:07 PM | |
Joined: 9/14/2009 Last visit: 9/23/2024 Posts: 41 Rating: (0) |
Thanks for your answer Mr.UMENCHO Regards |
Follow us on