4/27/2012 5:14 AM | |
Joined: 10/13/2008 Last visit: 11/11/2022 Posts: 41 Rating: (2) |
Hi Experts, I have the following configuration (see attached) and my question is How can my OPC Client ( PACKSRVA) communicate to a redundant WinCC Server (BOILERSRVA and B) which is also an OPC Server such that when BOILERSRVA is down, it automatically look for BOILERSRVB? Any Idea? if my configuration won't work, can you suggest a new configuration that will have the same effect? Thanks and best regards, Mike AttachmentSBM Server Server Connection.pdf (80 Downloads) |
5/2/2012 2:03 PM | |
Joined: 4/20/2010 Last visit: 4/22/2024 Posts: 38 Rating: (4) |
I'm sorry PCS 7 or WinCC is not able to handle redundant OPC Servers, may have a look at the following link, there you find a script which maybe helps you ;) |
This contribution was helpful to2 thankful Users |
Follow us on