2/18/2024 1:49 PM | |
Joined: 10/12/2021 Last visit: 4/18/2024 Posts: 8 Rating: (0) |
Dear Experts, I have a wincc v8.0 migrated backup, i want to get some data from third party (Yokogawa) OPC DA 2.0 Server. but when i try to search the server in my opc item manager in wincc tag managment, then it does not shows the required server. I have Completed DCOM settings in windows, my server PC is already on network. I tried with OPC Scout v10 (installed with simatic Net v16), the OPC DA server is accessible and i can read tags value also in the OPC scout. but in Wincc it does not found the server. In the older system with wincc v7.0, everything is working ok, the OPC DA server and their tags are accessible. I am wondering that the newer version of wincc supports OPC DA 2.0 or not. Or only the DCOM settings are not enough in windows 10 LTSC, does i have to do some work in registry ? I am attaching the screenshots of OPC scout and wincc opc item manager. Please check. what should i do to resolve the probelm. Regards Muktdir Attachmentscreenshots.zip (162 Downloads) |
Follow us on