5/21/2020 8:04 AM | |
Joined: 1/31/2020 Last visit: 10/11/2022 Posts: 19 Rating: (0) |
Hello! We have problems with the OPC server MAG8000. We have 52 flow meters that send a detailed water consumption report to the MAG8000 OPC server once a day, but when the MAG8000 OPC server connects to WinCC RT Professional v15.1, the server gives an error and data is not displayed. Data on the OPC MAG8000 comes in the “SQLite” format and then is saved in the “excel” format in the database folder, which is updated when new data arrives. Question: Is there a possibility of WinCC RT Professional v15.1 to work directly with “sqlite” files and receive information about expenses from them or with excel files to receive data on expenses?
AttachmentDataBase.pdf (173 Downloads) |
6/4/2020 8:03 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating: (169) |
Closed cause question posted twice. The second thread with the subject MAG8000 WinCCRT is published within the conference SIMATIC WinCC (TIA Portal). Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on