5/3/2024 11:58 AM | |
Joined: 3/11/2019 Last visit: 7/9/2024 Posts: 1511 Rating:
|
Hi, yes, via SIOME. FAQ also works with S7-1500. How do you change the Node ID identifier type of the nodes in the S7-1200 OPC UA Server from "Numeric" to "String"?regards sancruz |
Feedback appreciated, please rate |
|
5/7/2024 7:30 AM | |
Joined: 4/4/2024 Last visit: 7/11/2024 Posts: 16 Rating:
|
1. I exported the xlm file from the OPC server interface in TIA portal 2. Started SiOME and imported the xlm file. 3. Change namespace and choided all signal to be string and saved to xlm file 4. Tried to import the xlm file, but than I got a error, see below: |
6/14/2024 9:12 AM | |
Joined: 4/4/2024 Last visit: 7/11/2024 Posts: 16 Rating:
|
Thank you, I tried to install SiOME but could confuse, how is working. What I try to acchieve is that my OPC UA server in TIA portal is working that way that If I create a new server interface and drag tags to it, the tags will get the name of the symbol and not these ID. |
Follow us on