5/29/2023 4:12 PM | |
Joined: 5/25/2023 Last visit: 7/24/2023 Posts: 1 Rating:
|
Hello, I have a question about tools monitoring, I have some problems detecting the correct way to read tool life using simple client like uaexpert : in Sinumerik one NC variable I found in chapter 4.7.34 that tool/supervision I can find 2 parameters to check life: p2( remaining) and p5(starting). I'm trying to read this value with UAExpert. but I can't find a way: what information I need to explain in parameters to read P2 or P5 for a certain tool number in the parameter : NS2|String/Tool/Supervision/data[x,y,z]? SOLVED: I had solved my question : 1) read how many tools exist on CN ( NTOL) NS2|String/Tool/Catalogue/numTools 2) Read Tools Name NS2|String/Tool/Catalogue/toolIdent[1, NTOL] 3)Read Tool Number (T_ID) NS2|String//Tool/Catalogue/toolNo[1, NTOL] 4) Read Life parameter: NS2|String/Tool/Supervision/data[u1,cT_ID,2] ->Actual life ($TC_MOP2) NS2|String/Tool/Supervision/data[u1,cT_ID,5] ->Max Life ($TC_MOP11) NS2|String/Tool/Supervision/data[u1,cT_ID,1, 9 ] ->ALL ($TC_MOP1,$TC_MOP2,$TC_MOP3,$TC_MOP4,$TC_MOP11,$TC_MOP5,$TC_MOP6,$TC_MOP15) this project show me the way https://github.com/fpauker/toolmanagement/blob/master/sinumerik-opcua-readtooldata/ReadToolData.py ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/30/2023 10:57:14New subject after splitting Last edited by: U_f9cafc77-56b2-462a-84c3-49042d0a77a1 at: 06/06/2023 16:49:29 |
|
This contribution was helpful to
1 thankful Users |
Follow us on