6/30/2007 6:20 PM | |
Joined: 1/7/2006 Last visit: 12/23/2024 Posts: 2705 Rating:
|
Dear Woja, Normally a S7-300 CPU is only server and a CP343-1 Lean is also only server, so it can not innititate own initiatives. But with the open communication it might be possible to do something...... Look at the exampleHow is an open TCP communication connection established between an S7-300 PN CPU and a CP343-1, and how is data exchanged There is also a wizard Generating the Connection Data for the open TCP/IP Communication using the Open Communication Wizard I don't know if it works with a CP343-1 Lean, keep us posted |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on