11/22/2012 5:20 PM | |
Joined: 1/15/2010 Last visit: 8/9/2024 Posts: 19 Rating: (0) |
Hi guys, I'm trying to open an old S7 project with stand alone T400 inside (see the attachment). When I try to open a T400 project the system geve me back that I haven't got the Datebase of T400 221 (see the Attachment). Anybody can help me? Thaks a lot! Samuele
AttachmentT400_221_StandAlone_Error.zip (321 Downloads) |
11/22/2012 6:28 PM | |
Joined: 8/25/2006 Last visit: 11/6/2024 Posts: 2211 Rating: (280)
|
Hello. It seems like you try to open project that was created with newer version of DriveES, but your PC has older version installed. I think you have a drive (Simoreg or Simovert) with T400 andSPW420-program (axial winder). You need to install newer version of DriveES, the latest is5.5 SP1, or you may try to update only DriveMonitor to the latest version5.5 HF1. After updating, I think, you will get the latest database for T400.
|
11/23/2012 8:46 AM | |
Joined: 1/15/2010 Last visit: 8/9/2024 Posts: 19 Rating: (0) |
Thanks, I'm downloading the 5.5 HF1 version and I will install it with simoreg options. I will reply soon. Samuele
|
11/23/2012 9:54 AM | |
Joined: 1/15/2010 Last visit: 8/9/2024 Posts: 19 Rating: (0) |
I just installed the last DriveMon version. But the system is giving to me the same problem.. |
11/23/2012 10:09 AM | |
Joined: 1/15/2010 Last visit: 8/9/2024 Posts: 19 Rating: (0) |
For more clarity, I exported the DLN file and I renamed it in .txt. (In attachment the result).
AttachmentAvvolgitore_1.zip (336 Downloads) |
11/23/2012 10:59 AM | |
Joined: 1/15/2010 Last visit: 8/9/2024 Posts: 19 Rating: (0) |
Just tryed.. Same result but in different language. Seems the system needs the 221 or 222 T400 database.. ;(
|
Follow us on