5/21/2014 12:08 AM | |
Joined: 11/26/2011 Last visit: 6/29/2023 Posts: 508 Rating: (22) |
Its not possible with wincc flex. |
5/21/2014 7:17 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello Navnag, Ayman are right,
|
5/21/2014 9:44 AM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello Ayman Elotaify Thnks for your advise. However, I could open the WinCC Project created in WInCC Asia V6.2 by Using Project Migrator of WinCC V7.0. Now it opens in WInCC V7.0. We have installed it in another PC and it is working as standby as Main PC with WInCC Asia is giving problems and we do not have WinCC Asia available to install. Of course all tags are in special characters, but we are able to manage by using the Cross Reference of Tags as well using the "Find" option of Tag Editor. Could not open WinCC Flexible project though. ( At least not so far ... WinCCFlex Asia is not easily available as not a standard product in our country. ) STEP7 was much easier ( Just Deleted the Language file from the Global Folder ) Hope this help Cheers Navnag |
There is no such thing as the last bug in a program |
|
5/21/2014 9:51 AM | |
Joined: 11/26/2011 Last visit: 6/29/2023 Posts: 508 Rating: (22) |
Thanx for sharing the info. Its the biggest advantage of forum. |
5/30/2014 6:43 PM | |
Joined: 6/8/2013 Last visit: 7/18/2024 Posts: 158 Rating: (9) |
Dear Navang, It is possible to convet bye using language converter application of scada.
|
5/30/2014 6:50 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello Ashok Naphade Could you please provide some more information ... what you are trying to say. Thanks Navnag |
There is no such thing as the last bug in a program |
|
Follow us on