8/29/2009 10:24 AM | |
Posts: 116 Rating: (1) |
Hi, Can anyone suggest doecuments for understanding how siemens handles PWM output functionality? Regards Paresh |
8/30/2009 8:57 AM | |
Joined: 5/28/2008 Last visit: 1/2/2025 Posts: 4518 Rating: (841) |
Dear Paresh, You can generate pulse outputs or PWM via fast outputs using one of Siemens Compact CPUs. CPU312C: 2 channels pulse width modulation up to 2.5 kHz CPU313C / CPU313C-2PtP /CPU313C-2DP: 3 channels pulse width modulation up to max. 2.5 kHz CPU314C-2PtP /CPU314C-2DP: 4; Pulse width modulation up to 2.5 kHz You will found answer of your question "How to generate PWM from compact CPUs?"in chapter 5.7 in this manual: S7-300 CPU 31xC Technological Functions (CPU 312C, CPU 313C, CPU 314C) Best regards, |
Ayman Elotaify |
|
This contribution was helpful to1 thankful Users |
11/30/2017 1:04 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (174) |
New question published by Tholin is split to a separate thread with the subject Does the S7-300 6ES7 314-6EH04-0AB0 have a PWM?. Best regards |
12/2/2017 10:36 AM | |
Joined: 8/20/2009 Last visit: 11/6/2024 Posts: 80 Rating: (5) |
Hi Paresh, Please check below link for sample program on PWM. https://support.industry.siemens.com/cs/ww/de/view/18500266/en Also download manual from below link https://support.industry.siemens.com/cs/ww/en/view/12429336 |
Last edited by: Jen_Moderator at: 12/4/2017 10:54:19 AMInserted right links. Vishme. |
|
Follow us on