5/21/2007 9:33 AM | |
Joined: 4/24/2006 Last visit: 9/17/2024 Posts: 8738 Rating: (1168) |
Hello suk, Answers to your questions: 1) Not possible to make a backup of OP15 with Prosave and change it. , It's only possible to download it in an other OP15. 2) You should have the original project in Protool or Comtext. If you don't have the original project it will be very difficult. Advise start all over again. 3) Well here are some links to manuals: http://support.automation.siemens.com/WW/view/en/21084916 http://support.automation.siemens.com/WW/view/en/18796568 http://support.automation.siemens.com/WW/view/en/22900091 Best regards, Wizard |
6/11/2007 11:30 AM | |
Joined: 4/24/2006 Last visit: 9/17/2024 Posts: 8738 Rating: (1168) |
Hello, Have a look at this faq: http://support.automation.siemens.com/WW/view/en/213280 and in manual: http://support.automation.siemens.com/WW/view/en/1887570, you can look at page 9-3. Best regards, Wizard |
6/16/2007 9:16 AM | |
Posts: 17 Rating: (0) |
Dear sir |
6/18/2007 1:26 PM | |
Joined: 4/24/2006 Last visit: 9/17/2024 Posts: 8738 Rating: (1168) |
You are welcome I'm glad I could help. Best regards, Wizard |
Follow us on