Industry Online Support
Technical Forum
11/29/2012 6:50 AM | |
Joined: 8/25/2006 Last visit: 6/29/2024 Posts: 2207 Rating: (278) |
Hello. When you make a sturtup of new drive first time, you need to make an optimization runs at least for current and speed controller. During this optimizations drive determines the motor parameters and the parameters for current and speed controllers. If your drive will work with field weakening (with the speeds higher than rated speed) you need to execute optimization for field weakening. Look also at this thread: Knowledge Bank - 1 (Basics of AC and DC Drives)about basics of DC drives.
|
This contribution was helpful to1 thankful Users |
Follow us on