7/13/2015 2:05 PM | |
Joined: 5/20/2015 Last visit: 10/3/2024 Posts: 216 Rating: (3) |
hellow dear all, could anybody suggest me a optimum WINCC V7.3 SCADA software package, which could be sound cost effective, SOMEONE COATED ME VARIOUS SUB SOFTWARE WITH WINCC V7.3, MY REQUIRMENTS ARE AS FOLLOWS APPLICATION TYPE : TYPICAL BOILER APPLICATION, WITH AROUND 30 PID AND COULD BE EXTENDED UPTO 100 PID IN THE FURTHER IN THE FUTURE. ESTIMATED POWER TAGS PRESENTLY AROUND 2000 TAGS ARE ESTIMATED, CONSIDERING 8000 FOR THE SAKE OF THE FURTHER FUTURE ENHANCEMENT OF THE SYSTEM, STATION CPU WE HAVE CPU 1518F- 4 PN/DP WITH EXTENDED PROFINET I/O MODULE IM 155-6-PN HF SCOPE OF APPLICATION 1) CONTROLING AND MONITERING , 2)HISTORICAL AND REAL TIME TRENDS, 3)DATALOGING AND REPORT SHOULD BE GENERATE BY LOGGED DATA IN CUSTOM FORMATE. NOTE : THERE IS NO REQUIREMENT FOR RUNTIME USER ARCHIVE LIKE, RECIPE AND OTHER THINGS THANK YOU, HAVE A GREAT DAY..
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/13/2015 2:52:44 PMNew subject after splitting Let's do it... |
|
7/14/2015 3:10 PM | |
Joined: 5/20/2015 Last visit: 10/3/2024 Posts: 216 Rating: (3) |
THANK YOU bg2492,HAVE A GREAT DAY... |
Let's do it... |
|
6/13/2019 9:02 AM | |
Posts: 15 Rating: (0) |
Hello Gabbar, I have the same question but did not found any appropiate solution to the Problem i have nearabout same requirements with12 PIDs and about 500 estimated tags. Can you help me with the solution. Regards, Huzi saify |
Follow us on